IMX53 support details

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX53 support details

1,660 Views
debasishsaha
Contributor I

I am planning to work on IMX53. I wanted to know a few details prior to start my project

1) Is yocto build supported in IMX53?

2) What is the latest kernel supported by IMX53?

3) Is the build system supported on Ubuntu -14.04 or Ubuntu - 16.04?

Regards,

Debasish

Labels (1)
0 Kudos
Reply
1 Reply

1,424 Views
art
NXP Employee
NXP Employee

Q. Is yocto build supported in IMX53?

A. No, only ltib build is available.

Q. What is the latest kernel supported by IMX53?

A. The latest kernel that was supported for i.MX53 is 2.6.35

Q. Is the build system supported on Ubuntu -14.04 or Ubuntu - 16.04?

A. The only version of Ubuntu, tested for i.MX53 Linux BSP build, is 9.04. Other versions of Ubuntu have not been tested and may have build issues.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply