IMX53 support details

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX53 support details

1,661件の閲覧回数
debasishsaha
Contributor I

I am planning to work on IMX53. I wanted to know a few details prior to start my project

1) Is yocto build supported in IMX53?

2) What is the latest kernel supported by IMX53?

3) Is the build system supported on Ubuntu -14.04 or Ubuntu - 16.04?

Regards,

Debasish

ラベル(1)
0 件の賞賛
返信
1 返信

1,425件の閲覧回数
art
NXP Employee
NXP Employee

Q. Is yocto build supported in IMX53?

A. No, only ltib build is available.

Q. What is the latest kernel supported by IMX53?

A. The latest kernel that was supported for i.MX53 is 2.6.35

Q. Is the build system supported on Ubuntu -14.04 or Ubuntu - 16.04?

A. The only version of Ubuntu, tested for i.MX53 Linux BSP build, is 9.04. Other versions of Ubuntu have not been tested and may have build issues.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信