Hello,
I have built uboot, kernel and rootfs using LTIB for IMX53 QSB. I am using kernel 2.6.35. I am getting error as cannot get kernel image.
Please suggest.
My built kernel under /ltib/rootfs/boot is 3184904 bytes, but the u-boot command show 3184840 bytes....Is something wrong here?
I used following commands to flash u-boot and uImage respectively (It is a 8GB microsdcard)
$sudo dd if=u-boot.bin of=/dev/sdb bs=512 && sync && sync
$sudo dd if=uImage of=/dev/sdb bs=512 seek=2048 && sync && sync
MMC read: dev # 0, block # 2048, count 6144 partition # 0 ...6144 blocks read: OK## Booting kernel from Legacy Image at 70800000 ...Image Name: Linux-2.6.35.3-744-g27fdf7bImage Type: ARM Linux Kernel Image (uncompressed)Data Size: 3184840 Bytes = 3 MBLoad Address: 70008000Entry Point: 70008000Verifying Checksum ... Bad Data CRCERROR: can't get kernel image!MX53-LOCO U-Boot >