IMX53 Build for SMD (Sabre) Tablet

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX53 Build for SMD (Sabre) Tablet

1,073 Views
MichaelGale
Contributor II

Hi - I've got a working X11 build for the Sabre tablet, and I have a working OpenGL environment. When I build the IMX53 GPU samples from the GPU SDK, they run very slowly on the Sabre target (approx. 5-7 FPS for the pinball example). When I run the run the pre-installed examples in the Linux BSP for the Quick Start board, the performance is much better (approx. 27-33 FPS for the pinball example).


Any ideas for the significant difference in performance?

 

Thanks,

Michael

Tags (1)
0 Kudos
Reply
0 Replies