IMX515 display

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX515 display

2,351件の閲覧回数
wysockilukasz
Contributor II

I'm using custom board with imx51 with qnx system.
I need driver to display COM22H2P16ULC. It's a asynchronic display.
There is qnx driver in BSP for synchronic (RGB) display. I try to rewrite it to support
display I need but I can't even find which register I should set.

Lukasz

ラベル(3)
タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,167件の閲覧回数
Yuri
NXP Employee
NXP Employee

The following thread contains a patch, that may be useful.


https://community.freescale.com/message/406990
 

https://community.freescale.com/servlet/JiveServlet/download/405492-275392/iMX51_system80_LCD_patch....


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,167件の閲覧回数
Yuri
NXP Employee
NXP Employee

  I am afraid we do not have examples just for async display, sorry.
But I can send You directly (preliminary) app note, where DI programing for
GiantPlus GPM722A0 is considered . Hope it may help.

Please let me know Your e-mail. You may provide it as direct message to me.

The next app note (for i.MX31) provides details about the IPU async interface.
Let me remind i.MX31 IPU is not the same as i.MX51 IPU

http://cache.freescale.com/files/dsp/doc/app_note/AN4180.pdf


Have a great day,

Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信