IMX28 USB Package CRC ERROR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX28 USB Package CRC ERROR

1,535 Views
liuxing
Contributor II

Hi All,

    We encounter a very strange issue.We set up USB communication via IMX28 Host and device side.But we can see a lot of CRC errors from USB analyzer.

    We analyze the error package and find the  CRC value in the package is the CRC value befor final XOR.

    How to debug this issue?  Is there any register about the usb package CRC?

     pastedImage_1.png

    pastedImage_2.png

Labels (1)
0 Kudos
Reply
2 Replies

1,279 Views
liuxing
Contributor II

Hi All,

   We find that the all error packages are sent from usb device to usb host.

0 Kudos
Reply

1,278 Views
igorpadykov
NXP Employee
NXP Employee

Hi liu

one can look for steps of USB configuring in app note

http://cache.nxp.com/files/32bit/doc/app_note/AN4589.pdf

also please try to test i.MX28 usb module using testmodes

test, generating test patterns,(attached are for i.MX6),

one can add these codes to i.MX28 obds stmp_usb.c

Lab and Test Software (1)

"IMX_OBDS  : On-Board Diagnostic Suit for the i.MX28"

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MCIMX28EVKJ&fpsp=1&tab=Design_Tools_T...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply