IMX28 Micro SD Card on SSP2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX28 Micro SD Card on SSP2

2,002 Views
neeveehariharan
Contributor I

We have developed a custom board having Micro SD Card interfaced on IMX28 SSP2.

pinmux details are as given below,

static struct pin_desc mmc1_pins_desc[] = {

        { PINID_SSP2_SCK, PIN_FUN1, PAD_8MA, PAD_3V3, 1},

        { PINID_SSP2_MOSI, PIN_FUN1, PAD_8MA, PAD_3V3, 1},

        { PINID_SSP2_MISO, PIN_FUN1, PAD_8MA, PAD_3V3, 1},

        { PINID_SSP2_SS0, PIN_FUN1, PAD_8MA, PAD_3V3, 1},

        { PINID_SSP2_SS1, PIN_FUN2, PAD_8MA, PAD_3V3, 1},

        { PINID_SSP2_SS2, PIN_FUN2, PAD_8MA, PAD_3V3, 1},

}

struct imx_ssp_mmc_cfg ssp_mmc_cfg[1] = {

        {REGS_SSP2_BASE, HW_CLKCTRL_SSP2, BM_CLKCTRL_CLKSEQ_BYPASS_SSP2},

};

With this configuration, when we try to access micro SD Card, uboot console hangs.

Please share your inputs whether Micro SD Card can be interfaced with IMX28 SSP2 as above.

Thanks,

Hariharan.V.

0 Kudos
Reply
2 Replies

1,821 Views
igorpadykov
NXP Employee
NXP Employee

Hi Hariharan

one can look at example of ssp2 mmc configuration in digi ccardimx28js board

http://ftp1.digi.com/support/documentation/90001389_B.pdf

https://github.com/digidotcom/yocto-uboot/tree/v2013.04/master/board/digi/ccardimx28js

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,821 Views
neeveehariharan
Contributor I

I have gone through the example of "ccardimx28js" but it does not have info about SSP2 SD Card Access.

We have done the more deeper debugging in uboot, we found that clk_gate is not set again after SFTRST of SSP2.

Uboot hangs here at :

    /* Prepare for software reset */
    ssp_mmc_write(mmc, HW_SSP_CTRL0_CLR, BM_SSP_CTRL0_SFTRST);
    ssp_mmc_write(mmc, HW_SSP_CTRL0_CLR, BM_SSP_CTRL0_CLKGATE);
    /* Assert reset */
    ssp_mmc_write(mmc, HW_SSP_CTRL0_SET, BM_SSP_CTRL0_SFTRST);
    /* Wait for confirmation */
    while (!(ssp_mmc_read(mmc, HW_SSP_CTRL0) & BM_SSP_CTRL0_CLKGATE))
            ;

Please share your inputs to get SD Card access on SSP2.

Thanks,

Hariharan.V.

0 Kudos
Reply