IMX28 Linux BSP error on adding xorg

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX28 Linux BSP error on adding xorg

1,239件の閲覧回数
ganeshh
Contributor III

Hi,

I am having i.MX28 Evaluation Kit . I compiled Linux BSP source successfully and there is no problem in booting. But the board is not detecting USB keyboard so am unable to work i posted the issue in this thread (https://community.freescale.com/thread/323877) but i didnt get any fix till now.

In the log we can see the keyboard name is written as input device still am unable to type anything viard UART Debug port.


I tried to install Xorg thinking that while installing Xorg if it installs some dependency keyboard issue may get fixed but i got this error.How to fix this?


xorg.png

ラベル(3)
タグ(1)
0 件の賞賛
返信
0 返答(返信)