IMX27 Board is not Flashing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX27 Board is not Flashing

3,641件の閲覧回数
mohammedazlum
Contributor IV

We are using IMX27 (MCIMX27VOP4A-M72J-CTAM1325Z)

processor & PMIC-MC13783VK5 for G3 project. We need to

program the NOR flash(S29GL256N) using serial port(UART)

in our G3 board using Advanced tool kit(ATK). Some of the

boards are not able to program the NOR flash. I have

mentioned below the error showing on ATK Window while

programming the NOR flash.I have attached the Images.


Also , Some of the boards are suddenly got failed after 3-4

moths.After that , those boards are not able to re-flash & boot

( Initially Passed Boards).Those failed boards are impedance

& voltages,Clocks are proper.

Please suggest your Input.

Below i have mentioned issues while flashing.

1)Can't execute RAM kernal.

2)Connection error. Please reset the board and make sure the

board in

bootstrap mode.(Most of the time showing this issue)

3)Reset the target.

Note : While Flashing boards are in bootstrap mode.

Regards,

Azlum

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 返信

3,381件の閲覧回数
Yuri
NXP Employee
NXP Employee

Looks like memory (of i.MX27) is not working (or not initialyzed correctly)

0 件の賞賛
返信