IMX clock domain

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX clock domain

2,466件の閲覧回数
justinfei
Contributor I

When I read the datesheet of IMX8mq about the CCM.

1.I can't understand the clock domain usage and why the same clock have 4 domain setting(for example CCM_PLL_CTRLn has setting1 ~setting3).The 4 domain settings of one clock are working at the same time?

2.What is the usage of PLL domain settings and CCGR domain settings?

em......NXP's datasheets are hard to understand!

0 件の賞賛
返信
2 返答(返信)

2,155件の閲覧回数
tamotsu
Contributor V

Hi.

I also didn't understand that there are 4 domains.

"3.2.1.1 Features" of Resource Domain COntroller(RDC) in i.MX7D reference manual written as follews.

Assignment of cores, bus masters, peripherals, and memory regions to a resource domain.

Four of these ?

But it dosen't write which one is domain0.

0 件の賞賛
返信

2,454件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi

 

for domain usage one can look at description in sect.5.1.5.7 Access control, sect.5.1.6.2 PLL Interface,

sect.5.2.4.2 Low power mode

i.MX 8M Dual/8M QuadLite/8M Quad Applications Processors Reference Manual

 

Best regards
igor

0 件の賞賛
返信