IMX RT 1180

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX RT 1180

3,803 Views
SimoneColomboWEG
Contributor III

Hello,

i've some evk 1180, i've few problem with some pc to connect the target, in some pc (2) there is no way to connect evk for debugging, it finds MCU Link, but "0 available swd devices detected with MCUxpresso IDE" happen..

the same boards works to other pc.

the Version used is 25.x

pls help me to fix this problem on this pc ( we have also tried to use virtual machine on this pc but the problem is the same, also unistall and re-install all packages)

Thanks!

0 Kudos
Reply
10 Replies

3,665 Views
SimoneColomboWEG
Contributor III

FYI we are trying to install 25.9 but on all pc we have this issue after first login ask:

[info] Downloading file https://www.nxp.com/lgfiles/updates/mcuxpresso/JLink_Windows_V872_x86_64.exe using axios
[info] Installing SEGGER J-Link (8.72)...
[info] Executing and elevating command "C:\Users\colombos\AppData\Local\Programs\MCUXpressoInstaller\.cache\JLink_Windows_V872_x86_64.exe -Silent=1 -InstUSBDriver=1"
[info] Checking hash for file C:\Users\colombos\AppData\Local\Programs\MCUXpressoInstaller\.cache\debug_common-25.09.tar...
[info] Downloading Additional NXP debugger support from https://www.nxp.com/lgfiles/updates/mcuxpresso/debug_common-25.09.tar
[info] Downloading file https://www.nxp.com/lgfiles/updates/mcuxpresso/debug_common-25.09.tar using axios
[info] Installing Additional NXP debugger support (25.09)...
[info] Extracting debug_common-25.09.tar to C:\Users\colombos\.mcuxpressotools/debug_common-25.09
[info] Checking hash for file C:\Users\colombos\AppData\Local\Programs\MCUXpressoInstaller\.cache\LinkServer_25.9.134.exe...
[info] Downloading LinkServer from https://www.nxp.com/lgfiles/updates/mcuxpresso/LinkServer_25.9.134.exe
[info] Downloading file https://www.nxp.com/lgfiles/updates/mcuxpresso/LinkServer_25.9.134.exe using axios
[info] Installing LinkServer (25.9)...
[info] Executing and elevating command "C:\Users\colombos\AppData\Local\Programs\MCUXpressoInstaller\.cache\LinkServer_25.9.134.exe /VERYSILENT /SUPPRESSMSGBOXES"
[info] Checking hash for file C:\Users\colombos\AppData\Local\Programs\MCUXpressoInstaller\.cache\MCUXpresso_Config_Tools_v25.09_x64.exe...
[error] Error occurred while installing MCUXpresso Configuration Tools: self signed certificate in certificate chain. Skipping...
*** Installation error ***

0 Kudos
Reply

3,646 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @SimoneColomboWEG 

Thank you for your update and report!  ( @William_Weg  please use similar path for finding the JLink FW on Linkserver 25.9 :  C:\nxp\LinkServer_25.9.134\MCU-LINK_installer\scripts )

After first log in, I could install the version 25.9, So unfortunatelly I could not replicate the issue! but, I suggest to install Linkserver package  directly from  this page https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools...

Please let me know your results, guys

Diego

 

0 Kudos
Reply

3,667 Views
William_Weg
Contributor I

Hi, I a Simone's collegue I have this problem in my pc and I Installed last version of LinkServer, on-board LPC55 but nothing changes. I want understand where i can find il JlinkFW mentioned in "try testing with JLink FW", thaks

0 Kudos
Reply

3,654 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @William_Weg 

Please refer to the below image!

diego_charles_0-1759878654051.png

Diego

0 Kudos
Reply

3,459 Views
William_Weg
Contributor I

Hi Diego,

 I'm sorry but in any case doesn't work.

 

William_Weg_0-1760361481995.png

jp3 is close for isp mode

0 Kudos
Reply

3,458 Views
William_Weg
Contributor I

Link flash with GUI is correctly connected 

William_Weg_0-1760362265045.png

 

0 Kudos
Reply

3,432 Views
diego_charles
NXP TechSupport
NXP TechSupport

 Hi @William_Weg 

thank you for your update!

I was able to update FW on my side

diego_charles_0-1760387735658.png

I placed  a jumper on JP3 and power cycled the whole EVK. 

 

diego_charles_2-1760387948213.png

I am using this schematic revison: 

 

diego_charles_4-1760387997973.png

What is the schematic revision that you are using? Does update also fails with CMSIS DAP?

Thank you, 

Diego

 

 

0 Kudos
Reply

3,343 Views
SimoneColomboWEG
Contributor III
Goodmorning Diego,
we have just tried to program debugger as Segger and works but our target is using like CMSIS Link debug.
I've an update maybe to understand the behaviour,we use an SVN server to share the code in the team, we share oonly the project folder, the metadata and not the debug folder, for me and for other user(we have just adnn a now colleague yesterday, as i said, all works good) for other two not we have the problem above. BUT the weird comes here: if i export the project via zip(project and reference form mcuxpresso function) with no debug folder nothig works as like SVN, BUT if i export the project and reference with debug folder all works also on a William pc.
the other weird behaviour is when not works if i jump to a works peoject i need to reset the debugger, is looks like stuck...
0 Kudos
Reply

3,682 Views
SimoneColomboWEG
Contributor III

Thanks Diego,

all pc with this problem is winodws 11 pro 24H2 build 26100.6584 the same as mine (that works). we have just tried to download the latest link server, the Lpc55 onboard is the latest version. as i said i can use (with another collegue) the boards with no problem, it runs correctly but the other two collegue there is no way to works!

what i can do? 

FYI i'm working on a 24.x skd version (because i can't update for TSN support) and works correctly also with this version.

3,757 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @SimoneColomboWEG 

Please try to install the latest version of the Linkserver on that machine. Lets see if installing the drivers makes a difference. What is your OS? Do all the machines have the same OS and version? 

Also, try to  update the on-board LPC55 to run the latest version of CMSIS DAP. If this does not make any change at all, try testing with JLink FW. Let me know if you need more steps for this!

Diego

0 Kudos
Reply