IMX-MKIMAGE u-boot-atf.bin file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX-MKIMAGE u-boot-atf.bin file

3,110 Views
lsanvictores
Contributor I

I'm attempting to build a custom image for the imx8qxp board. When I follow the steps in https://community.nxp.com/docs/DOC-343178 to create the bootable image, it's not clear to me how to generate u-boot-atf.bin. I'd appreciate any direction to complete this step.

0 Kudos
Reply
1 Reply

2,606 Views
igorpadykov
NXP Employee
NXP Employee

Hi Lacy

also one can look at description of building images from third parties

Build Apalis iMX8/Colibri iMX8X Boot Image/Linux from Scratch 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply