IMX Android 8.0.0 add yuyv format support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX Android 8.0.0 add yuyv format support

1,328 次查看
wangaizhi
Contributor I

I download Android 8.0.0 Oreo (O8.0.0_1.0.0, 4.9 kernel)  from Official website。We connected a camera with DVP interface,and need to get the raw data in YUYV format in the android application layer。I modified the camera file to add yuyv support in vendor\nxp-opensource\imx\libcamera3\InfraredCsi.cpp as follows:

sensorFormats[index] = v4l2_fourcc('Y', 'U', 'Y', 'V');
availFormats[index++] = v4l2_fourcc('Y', 'U', 'Y', 'V');
mSensorFormatCount = changeSensorFormats(sensorFormats, mSensorFormats, index);
if (mSensorFormatCount == 0) {
   ALOGE("%s no sensor format enum", __func__);
   close(fd);
   return BAD_VALUE;
}

Also I add print in vendor\nxp-opensource\imx\libcamera3\Metadata.cpp :

m.addInt32(ANDROID_SCALER_AVAILABLE_FORMATS,
sensor.mAvailableFormatCount,
sensor.mAvailableFormats);
int i = 0;
for(i = 0; i < sensor.mAvailableFormatCount; i++)
{
   ALOGE("====waz: mAvailableFormats = %d\n", sensor.mAvailableFormats[i]);
}

Only one value is printed here is 20, represents the yuyv format。

But use the camera2 interface to view in the application layer, and there is no such format。

Add yuyv support, what else needs to be modified?

Thanks!

0 项奖励
回复
1 回复

1,273 次查看
joanxie
NXP TechSupport
NXP TechSupport

what board and bsp are you talking about?

0 项奖励
回复