IMX.6 boot from SD card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX.6 boot from SD card

882 Views
aydinalci
Contributor II

Hello, I bought a IMX.6QP SABRE module just a few days ago and there is no

SD card to boot it inside of the pack which is the delivered.

So i am tring to boot it with my personal SD card and i downloaded latest

BSP filse from the internet but i did not succeed it. So please, give me

some advice how i have to do with my personal SD card and windows OS

dekstop.

Thanks.

0 Kudos
Reply
1 Reply

744 Views
igorpadykov
NXP Employee
NXP Employee

Hi AUDIN

seems most easy way is to use mfg tools and eMMC, please use

mfgtool2-yocto-mx-sabresd-emmc-6qp.vbs script :

Programmers (Flash, etc.) (2)

IMX6_L4.1.15_MFG_TOOL (REV L4.1.15_1.0.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply