IMX 6 SOLO PWM Output control

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX 6 SOLO PWM Output control

1,351 Views
pradeepn
Contributor I

We are trying to drive the buzzer in our design through PWM output line from solo processor .Now The buzzer requires minimum of 5 V .But PWM output is not enough to drive the buzzer . I wonder is there any possiblity that we can disable the internal pull-up and provide external pull-up of 5V to the PWM and drive that?

With regards ,

PRADI

Labels (2)
0 Kudos
Reply
1 Reply

1,224 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi,

No , you can not do that. Here you can do as follow design:

67BC99F1.PNG

Or you can use the LEVEL SHIFT circuit design.
Have a great day,
Rita

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply