IMX.6 Kitkat 4.4 CTS Keychain HAL failure.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX.6 Kitkat 4.4 CTS Keychain HAL failure.

2,151件の閲覧回数
adamduskett
Contributor II

Hey guys, we are building a tablet based on the IMX.6 processor and we are running into a error with one of the tests.  Specifically:

android.keystore.cts.KeyChainTest#testIsBoundKeyAlgorithm_RequiredAlgorithmsSupported FAIL

junit.framework.AssertionFailedError: RSA must be hardware-backed by a hardware-specific Keymaster HAL

at android.keystore.cts.KeyChainTest.testIsBoundKeyAlgorithm_RequiredAlgorithmsSupported(KeyChainTest.java:37)

at java.lang.reflect.Method.invokeNative(Native Method)

at android.test.AndroidTestRunner.runTest(AndroidTestRunner.java:191)

at android.test.AndroidTestRunner.runTest(AndroidTestRunner.java:176)

at android.test.InstrumentationTestRunner.onStart(InstrumentationTestRunner.java:554)

at android.app.Instrumentation$InstrumentationThread.run(Instrumentation.java:1701)


Looking around it doesn't seem like there is a keymaster hal for the IMX.6 platform.  Is this true or am I just blind?


Thanks!

ラベル(3)
0 件の賞賛
返信
3 返答(返信)

997件の閲覧回数
haoranwang
NXP Employee
NXP Employee

Hi Adam,

     Sorry for that. Our Android Kitkat BSP need trustzone to support secure hard module. But currently we are not support trustzone.

BRs

Haoran

0 件の賞賛
返信

997件の閲覧回数
leonlin
Contributor I

Hi Haoran,

             We meet the same issue, will FREESCALE BSP 4.4.3  support the trustzone soon? or we just ignore this CTS test error because you have no plan to support the trustzone?

0 件の賞賛
返信

997件の閲覧回数
haoranwang
NXP Employee
NXP Employee

Hi Leon,

     Please ignore it. Freescale BSP 4.4.3 doesn't support it neither.

     Thanks!

BRs,

Haoran