Hello,
I am facing some show stoppers in my project.
We have one chip processor, we need to communicate it through I2C channel 2.
The board is designed like ,that chip is connected to Channel 2.(we have three i2c channels i2c0,i2c1,i2c2)
So When we tried to execute below code, we got write error
fd = open("/dev/i2c-2", O_RDWR);
ioctl(fd, I2C_SLAVE, I2C_ADDR);
char buffer[5];
buffer[0] = 0x0;
printf("Value : %c\n", buffer[0]);
float data;
char channel;
res = write(fd, buffer, 1);
if (res < 0) {
printf("-- ");
printf("Error writing file: %s\n", strerror(res));
} else {
printf("****%02x **", i + j);
data = (float) ((buffer[0] & 0b00001111) << 8) + buffer[1];
printf("%u\n", buffer[0]);
data = data / 4096 * 5;
channel = ((buffer[0] & 0b00110000) >> 4);
printf("Channel %02d Data: %04f\n", channel, data);
}
But when we changed our hardware like the chip connection redirected to channel 0,and tried the above code,(with change in open("/dev/i2c-0", O_RDWR)) write was success.
I have modified include\mach\iomux-mx6q.h , arch\arm\mach-mx6\board-mx6dl_sabresd.h to add the mux and pad register values.
Still no change.
Could anyone please help me to solve this issue??
Regards
Divya R Dharan