IMAX8 PCIE_REFCLK100M

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMAX8 PCIE_REFCLK100M

1,583 Views
ceng_guanghui
Contributor II

The IMAX8 PCIE_REFCLK100M can use as a resource for output?or need external clock input. 

Thank you

0 Kudos
Reply
1 Reply

1,526 Views
igorpadykov
NXP Employee
NXP Employee

Hi

>The IMAX8 PCIE_REFCLK100M can use as a resource for output?or need external clock input.

both options can be used.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply