IM.X35 no serial(console) input (3.11.1)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IM.X35 no serial(console) input (3.11.1)

Jump to solution
1,622 Views
maxvankessel
Contributor II

I'm using an I.MX35 SOC with the freescale linux mainline  (3.11.1).

I'm unable to receive any bytes from the serial input, the serial input/output (UART3) is connected to the console.

Someone an idea what is wrong?

Labels (1)
0 Kudos
Reply
1 Solution
1,553 Views
maxvankessel
Contributor II

Thanks,

Both Tx and Rx were configured for different pins.

Transmit was working (not configured), but receiver wasn't doing a thing.

Fixed the problem by changing the pins to the correct RS232 pins.

View solution in original post

0 Kudos
Reply
3 Replies
1,554 Views
maxvankessel
Contributor II

Thanks,

Both Tx and Rx were configured for different pins.

Transmit was working (not configured), but receiver wasn't doing a thing.

Fixed the problem by changing the pins to the correct RS232 pins.

0 Kudos
Reply
1,553 Views
fabio_estevam
NXP Employee
NXP Employee

Does U-boot work? It would help if you could post your board file, boot logs, etc.

0 Kudos
Reply
1,552 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Max,

I recommend you first to check the serial configurations, the speed is 115200 for example. And make sure if your board is working.

Best Regards

Dan

0 Kudos
Reply