IEEE1588 on i.MX6Solox

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IEEE1588 on i.MX6Solox

跳至解决方案
733 次查看
linzhou
Contributor II

Hi bpe,

Our project uses the i.MX6SoloX processor. In the IEEE1588 application, I didn't find more references in the datasheet and reference manual.I have the following questions that need your support.:
1. I understand IEEE1588, there should be similar pins such as 1588_CLK_IN, 1588_PULSE_OUT, but I have not found similar pins in the i.MX6SoloX processor. The pins related to IEEE1588 are only ENETn_1588_EVENTn_IN and ENETn_1588_EVENTn_OUT. How to connect these pins correctly?
2. Do I need to add an external high precision reference clock source separately? Is it possible to pass the ENETn_1588_EVENTn_IN pin if needed?
3.Is the 1 PPS signal output directly through the ENETn_1588_EVENTn_OUT pin?

 

Thanks very much for your reply!

0 项奖励
回复
1 解答
665 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  please refer to the following: https://community.nxp.com/thread/486148 

Regards,

Yuri.

在原帖中查看解决方案

0 项奖励
回复
1 回复
666 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  please refer to the following: https://community.nxp.com/thread/486148 

Regards,

Yuri.

0 项奖励
回复