IBIS Model IMX6Q Series ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IBIS Model IMX6Q Series ?

2,357 Views
peteramond
Contributor V

Hi All,

I'm using following attached IBIS model which is downloaded from NXP to run on HyperLynx signal integrity simulation. But after adding it to the library path and when I try to close the window it shows following message. Seems like it is not taking the IBIS model correctly. And also when I go to edit model file I can see PCIE_RXM are not connected. 

IBIS model >> https://www.nxp.com/search?category=softwaretools&keyword=IBIS&start=40

Anyone encounter this problem ? Can I have the correct IBIS file for part number >>

MCIMX6Q6AVT10AC

pastedImage_1.png

Regards,

Peter.

Labels (4)
0 Kudos
Reply
1 Reply

2,164 Views
igorpadykov
NXP Employee
NXP Employee

Hi Peter

unfortunately these signals (PCIe) are not supported by i.MX6Q ibis model

according to Table 7-6. i.MX6 pins not supported by IBIS

IMX6DQ6SDLHDG, Hardware Development Guide for i.MX 6Quad, 6Dual, 6DualLite,

6Solo Families of Applications Processors

https://www.nxp.com/webapp/Download?colCode=IMX6DQ6SDLHDG 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply