I2C Multi master support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I2C Multi master support

3,545件の閲覧回数
NithinkumarN
Contributor II

Hi All,

I'm working on i.MX6Q processor custom board.

I will use L3.0.35_4.1.0 freescale release code.

I need to test I2C multi master in my platform.

Please let me know , this feature is already present in existing I2C driver of L3.0.35_4.1.0 release linux kernel.

Thanks and Regards,

Nithin

ラベル(2)
0 件の賞賛
返信
2 返答(返信)

3,240件の閲覧回数
art
NXP Employee
NXP Employee

The only feature of the L3.0.35 BSP I2C driver that can help to support the multi-master I2C bus is the possibility to generate the Arbitration Lost interrupt in case of losing bus arbitration during the master data transfer. No other features are provided.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,240件の閲覧回数
NithinkumarN
Contributor II

Hi All,

Any update on above query, Please let me know as soon as possible since I'm in implementation stage.

Thanks and Regards,

Nithin

0 件の賞賛
返信