I.mx6 processor-emmc flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.mx6 processor-emmc flash

1,340件の閲覧回数
rakshatan
Contributor I

Hi Everyone,

I am working on i.MX6Q processor(SABRE Platform for Smart Device) .Could you please tell me, through which bus the SANDISK emmc flash is connected to processor.

Thank you

0 件の賞賛
返信
1 返信

1,252件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Rakshata

emmc is conected to i.MX6Q SD4 port (uSDHC module),

connections are given on p.5 spf-27392 Sabre schematic

Schematics (1)

Design files, including hardware schematics, Gerbers, and OrCAD files. (REV C5)

SABRE for Smart Devices Reference Design|NXP

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------