I cannot get nodejs latest version - imx6ulevk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I cannot get nodejs latest version - imx6ulevk

2,120 Views
gbassi1
Contributor II

Hello,

The repo approved by nxp in the Yocto manual documentation is not the latest one (master branch), but th rocko one. Why is this?

In OpenEmbedded Layer Index:

Checking rocko or master branch, it is only available version 7.10.0 for meta-nodejs (OpenEmbedded Layer Index - meta-nodejs )

In OpenEmbedded  Recipes Index:

  • For rocko: v8.4.0
  • For master branch: v10.15.3

Also, in recipes, there is no npm package and I need that too.

So, my questions are:

  1. Why the latest branch suggested by i.MX_Yocto_Project_User's_Guide is not the latest one? It repo sync brings rocko.
  2. Should I repo sync the master? How do I do that?
  3. How can I get latest npm as well? (v6.x.x) The layer meta-nodejs includes nodejs-npm as a package but it is not in the latest version.

Thanks

Labels (4)
0 Kudos
Reply
1 Reply

1,859 Views
b36401
NXP Employee
NXP Employee

You may add a layer to an image by adding following line to the conf/local.conf file inside the build directory, and then baking the image.
IMAGE_INSTALL_append = “ nodejs”

Whenever you want to see which packages are available on the BSP you can run:
bitbake -s

0 Kudos
Reply