I am looking for a processor which can support audio input and output, camera flash memory upto 4 GB and usb connectivity. please help me finding the right processro.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I am looking for a processor which can support audio input and output, camera flash memory upto 4 GB and usb connectivity. please help me finding the right processro.

1,255件の閲覧回数
raushanverma
Contributor I

​​I am looking for a processor which can support audio input and output, camera flash memory upto 4 GB and usb connectivity. please help me finding the right processro.​

0 件の賞賛
返信
1 返信

1,203件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi,

If you are looking for a multimedia-oriented processor, you could refer to the i.MX6 Series of Applications Processors, at the following link:

http://www.freescale.com/imx6

You could take a look at the SABRE Platform for i.MX6 family, which has two camera interfaces, audio input and output, USB On-The-Go port, etc:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREPLAT

There are other third-party low cost boards based on the i.MX6 families, like SABRE Lite, RiOTboard, Udoo and others. You could refer to the “Evaluation/Development Boards and Systems” menu of the “Software & Tools” tab of the i.MX6 Product Summary Page at the following link:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&fpsp=1&tab=Design_Tools_Tab

Hope this will be useful for you.
Best regards!
/Carlos

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信