I.Mx secuirty reference module documents

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.Mx secuirty reference module documents

2,574 Views
ravikiranhv
Contributor I

Hi,

I am using I.MX 6 board.

Please can you provide I.Mx secuirty reference module? I want to use securiry(AES/DES) features of I.Mx in Linux.

Thank you

Labels (1)
Tags (4)
0 Kudos
Reply
2 Replies

2,089 Views
ravikiranhv
Contributor I

Dear Freescale,

I am using I.MX 6 board with Linux 3.10.53.

Please can you provide I.Mx security reference manual for this board? I want to use security(AES/DES) features of I.Mx in Linux.

Thank you

0 Kudos
Reply

2,089 Views
Yuri
NXP Employee
NXP Employee

  Please use the i.MX6 Security Reference Manual

http://www.freescale.com/webapp/sps/download/mod_download.jsp?colCode=IMX6DQ6SDLSRM&appType=moderate...

Or try the link "MX6DQ6SDLSRM Security Reference Manual for i.MX 6" on the next Summary Page.

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&fpsp=1&tab=Documentation_Tab

As for Linux, please refer to "i.MX_6_Linux_High_Assurance_Boot_(HAB)_User's_Guide.pdf" and
"i.MX_6_Linux_Reference_Manual.pdf" in documentation.

http://www.freescale.com/webapp/Download?colCode=L3.10.53_1.1.0_LINUX_DOCS

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX6_SW


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply