Hi.
The following error occurred when I tried to stream video from two cameras(720p@60fps) with gstreamer.
"mx6s-csi 30a90000.csi1_bridge: mx6s_csi_irq_handler Hresponse error detected"
(BSP : 4.9.51_imx8m_ga)
And the frequency of occurrences is 1-2 in five on average.
For this error, I had checked the file that 'drivers/media/platform/mxc/capture/mx6s_capture.c', and I got It occurs when the bit BIT_HRESP_ERR_INT is on.
So, I want to know the meaning of this error and the information of CSI_CSISR register or the solution for this error.
(I couldn't found the meaning of this error and information of CSI_CSISR in any manual for i.mx8.)
Thanks!
已解决! 转到解答。
Hi dokim
HRESP_ERR_INT - AHB Bus Response Error Interrupt:
AHB Bus response error interrupt is generated when a bus error is detected.
similar to i.MX7D CSI_CSISR register described in sect.13.3.7.7 CSI Status Register (CSI_CSISR)
Reference Manual.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi dokim
HRESP_ERR_INT - AHB Bus Response Error Interrupt:
AHB Bus response error interrupt is generated when a bus error is detected.
similar to i.MX7D CSI_CSISR register described in sect.13.3.7.7 CSI Status Register (CSI_CSISR)
Reference Manual.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
one can check Linux Manual with description of drivers:
https://www.nxp.com/webapp/Download?colCode=L4.9.88_2.0.0_LINUX_DOCS
Best regards
igor