I.MX8M Errata -- 2N14W ID No. e9165

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX8M Errata -- 2N14W ID No. e9165

Jump to solution
945 Views
yyc1975
Contributor III

Hello,

 

Does e9165(eCSPI: TXFIFO empty flag glitch can cause the current FIFO transfer to be sent) also affect UART if I set ECSPI2 as UART4?

We connect UART4 to a RS485/RS422/RS232 Multiprotocol transceiver(F81439AN) and got an issue with TXFIFO works abnormal.

 

IOMUXC_SW_MUX_CTL_PAD_ECSPI2_SS0  --> ALT1_UART4_RTS_B

IOMUXC_SW_MUX_CTL_PAD_ECSPI2_MISO  --> ALT1_UART4_CTS_B

IOMUXC_SW_MUX_CTL_PAD_ECSPI2_MOSI   --> ALT1_UART4_TX

IOMUXC_SW_MUX_CTL_PAD_ECSPI2_SCLK   --> ALT1_UART4_RX

0 Kudos
Reply
1 Solution
933 Views
igorpadykov
NXP Employee
NXP Employee

Hi yyc1975

 

e9165 (eCSPI: TXFIFO..) affects only ecspi, not uart.

 

Best regards
igor

View solution in original post

0 Kudos
Reply
1 Reply
934 Views
igorpadykov
NXP Employee
NXP Employee

Hi yyc1975

 

e9165 (eCSPI: TXFIFO..) affects only ecspi, not uart.

 

Best regards
igor

0 Kudos
Reply