I.MX7 is supported MIPI Camera?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX7 is supported MIPI Camera?

2,252件の閲覧回数
viswanathreddy
Contributor I

Hi All,

would you please any one provide the I.Mx7 camera bring up document or path.

I.Mx6 they used IPU but I.MX7 is ISP

Please provide the I.Mx7 boundary devices bring up documets.

Thanks

Viswa

ラベル(2)
0 件の賞賛
返信
1 返信

1,890件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Viswa

OV5647 mipi camera was verified on iMX7D board.

https://community.nxp.com/thread/395858

also one can use camera module from Boundary Devices

OV5640 Camera Module for i.MX6 boards 

As for documentation one can refer to Chapter 20 MIPI CSI2 Driver

attached Linux Manual.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信