I.MX6dual PCIE Function application

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX6dual PCIE Function application

1,205件の閲覧回数
tommyduan
Contributor III

1、PCIE interface supports video transmission?

2、Does PCIE support master-slave Settings?

3、What is the maximum rate supported by PCIE?

4、What functions does the underlying software PCIE currently support?

0 件の賞賛
返信
1 返信

1,191件の閲覧回数
art
NXP Employee
NXP Employee

1. Any kind of data, including video, can be transferred over a PCIe link.

2. Yes, the PCIe controller of i.MX6Dual can operate as either Root Complex or Endpoint.

3. The i.MX6Dual PCIe interface conforms to the PCIe v.2.0 specification that provides 5Gbit/s data throughput.

4. The Linux BSP contains the PCIe driver. For details, please refer to the corresponding chapter of the i.MX Linux Reference Manual document:

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

Best Regards,
Artur

0 件の賞賛
返信