I.MX6dual PCIE Function application

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6dual PCIE Function application

1,219 Views
tommyduan
Contributor III

1、PCIE interface supports video transmission?

2、Does PCIE support master-slave Settings?

3、What is the maximum rate supported by PCIE?

4、What functions does the underlying software PCIE currently support?

0 Kudos
Reply
1 Reply

1,205 Views
art
NXP Employee
NXP Employee

1. Any kind of data, including video, can be transferred over a PCIe link.

2. Yes, the PCIe controller of i.MX6Dual can operate as either Root Complex or Endpoint.

3. The i.MX6Dual PCIe interface conforms to the PCIe v.2.0 specification that provides 5Gbit/s data throughput.

4. The Linux BSP contains the PCIe driver. For details, please refer to the corresponding chapter of the i.MX Linux Reference Manual document:

https://www.nxp.com/design/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applicat...

Best Regards,
Artur

0 Kudos
Reply