Hi all,
I now have the i.mx6UL IC that is suppose to run on 696MHz with me now (MCIMX6G2AVM07AB).
However, it seems that it is still running at 528MHz max.
From the kernel source code (kernel version 3.14.52), the operating points seems like limited to 528MHz only (arch/arm/boot/dts/imx6ul.dtsi file).
operating-points = <
/* kHz uV */
528000 1175000
396000 1025000
198000 950000
>;
fsl,soc-operating-points = <
/* KHz uV */
528000 1175000
396000 1175000
198000 1175000
>;
May I know is there any patches for kernel 3.14.52 that allows the imx6ul to runs at 698MHz? Anything else that i need to change in the kernel source code to make it runs at 696MHz?
Thank you.
Regards,
Tee
Hi Tee
one can look at Linux 4.1.15_2.0.2 Patch "i.MX 6ULL@800M" on link
https://www.nxp.com/products/microcontrollers-and-processors/arm-based-processors-and-mcus/i.mx-appl...
and make similar modifications for 698 option. Unfortunately I am not aware of such patches for kernel 3.14.52.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------