How to increase RPMSG baud rate on iMX6SX?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to increase RPMSG baud rate on iMX6SX?

1,451 Views
liushuo
Contributor I

I'm testing the rpmsg on iMX6SX using the rpmsg tty driver "imx_rpmsg_tty.ko". The communication between the A9 coreand M4 core is successful, but the data rate seems very low. I checked the settings of the "ttyRPMSG" device, and found the default buad rate is only 38400:


# stty -F /dev/ttyRPMSG
speed 38400 baud; line = 0;
intr = ^C; quit = ^\; erase = ^?; kill = ^U; eof = ^D; eol = <undef>;
eol2 = <undef>; swtch = <undef>; start = ^Q; stop = ^S; susp = ^Z; rprnt = ^R;
werase = ^W; lnext = ^V; flush = ^O; min = 1; time = 0;
-brkint -imaxbel

How do I increase this baud rate(for example, 115200)?

Is there any alternative way to achieve a faster communication speed between the A9 core and M4 core, instead of using the tty interface? 

Labels (1)
0 Kudos
Reply
1 Reply

1,025 Views
BiyongSUN
NXP Employee
NXP Employee

Please follow the instructions in i.MX_Linux_Reference_Manual.pdf of BSP release

Untitled.png