If using JTAG to load my program (i.MX6UL based device) to RAM, USB works. But the same program flashed to QSPI NOR and loaded by NXP bootrom code, USB does not work. The host PC does not even detect our device. OTG1 UTMI PHY Control 0 Register is 0 indicates clock invalid. Any suggestions? Thanks.
CCGR6 is enabled. I have also enabled CCM_ANALOG_PLL_USB1 according the procedure by NXP document:
1. Enable PLL.
2. Set POWER bit to power-up the PLL.
3. Wait for PLL_LOCK bit to assert.
4. Clear BYPASS bit. This will switch the PLL output from Bypass clock to PLL output clock.
5. Set EN_USB_CLKS. This enables the PLL’s 9-phase clock output for the PHY
It is still not working.
I always cycle power before loading by JTAG. So I think the i.MX6UL bootrom code runs first and initialize the USB as a HID device. My code then reinitialize the USB to another device. I guess the bootrom code help me some how. When configured to boot from QSPI, the bootrom loads code from QSPI and never initialize the USB.
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		is it working with uboot:
in uboot/include/configs/mx6ul_14x14_evk.h set #define CONFIG_CMD_USB
Best regards
igor
 
					
				
		
 igorpadykov
		
			igorpadykov
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi Qing
please check that usb clocks are enabled in CCM_CCGR6
register.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------