I.MX6Q SABRE BOARD eMMC boot error.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6Q SABRE BOARD eMMC boot error.

2,164 Views
oguzyaz
Contributor I

Hi,

we can boot on SD3 with SD Card. It's OK. But ı want to boot from eMMC4.4(SDIN5C2-8G) memory on board. I use MFG Tool for loading.

After loading u-boot,kernel and OS, the system doesn't boot, doesn't change anything in PUTTY.

Can you help me ?

Labels (1)
0 Kudos
Reply
3 Replies

1,866 Views
SergioSolis
NXP Employee
NXP Employee

Are you setting the dip switches to boot from EMMC?, these are: 1,2,4,6,7 (ON)

0 Kudos
Reply

1,866 Views
oguzyaz
Contributor I

Yes of course.

I am going with the i.MX_6Dual6Quad_SABRE-SD_Linux_User's_Guide.pdf .

But I solved the problem like this;

I boot the system from SD card and when ı see 'Uncomperresing kernel' and 'loading kernel' in PUTTY, ı take out the SD card and system continue booting on eMMC.

I think U-boot is problem.

0 Kudos
Reply

1,866 Views
Yuri
NXP Employee
NXP Employee

What about U-boot environment : SD and eMMC ones are very similar : for SD / MMC "mmc dev 2" is used ; for eMMC - "mmc dev 3".

0 Kudos
Reply