I.MX6Q IRQ ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

I.MX6Q IRQ ?

2,799 次查看
grégorycascio
Contributor I

Bonjour a tous,

Je suis en possession d'une carte de chez Emtrion (Dimm MX6) dotée d'un processeur freescale IMX6Q

On m'a demandé pour mon sujet de stage de tester le processeur sur ses performances, surtout au niveau des IRQs.

Dans mon entreprise on a besoin d'une IRQ se déclenchant toute les 500µs avec un état haut d'une durée de 150µs environ.

Je viens vers vous car je ne sais pas comment gérer les IRQs (je sais juste a quoi sers une IRQ mais rien de plus).

Je voulais savoir les démarches a suivre pour piloter une IRQ de la carte.

Merci d'avance

Cordialement

标签 (1)
0 项奖励
回复
3 回复数

2,634 次查看
grégorycascio
Contributor I

Sorry my english is bad. I try to make it compehensible

I am in possession of a card from Emtrion (Dimm MX6) with a freescale processor IMX6Q


I was asked for my company subject to test the processor performance, especially in terms of IRQs.
In my company we need an IRQ is triggering all the 500μs with a high state for a period of approximately 150μs.


I come to you because I do not know how to handle IRQs (I know just what has been using an IRQ but nothing more).


I wanted to know the steps to follow to control an IRQ to the card.


Thank you in advance

Best regaurd

0 项奖励
回复

2,634 次查看
varsmolta
Contributor V

is the IRQ an input to or an output from your card? I assume it is an input to your card that you need to handle.

Will you be handling your interrupt in kernel or user space?

If it is an input, according to page 19 of the manual here:

http://www.emtrion.com/doc/DIMM-MX6x_HW_V003en.pdf

you will have to configure one of the the associated GPIO as an input. See here how to do so for user space or kernel space configurations:

http://processors.wiki.ti.com/index.php/GPIO_Driver_Guide

Note: even though the above link is TI specific, the gpio_to_irq(), request_irq() and set_irq_type() are generic linux constructs and should apply to freescale linux kernel as well

2,634 次查看
AlbertT
Contributor V

You should speak in english.

0 项奖励
回复