I.MX6 ULL eMMC VDD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX6 ULL eMMC VDD

2,171件の閲覧回数
massimo2
Contributor III

Hello

What is the supply voltage used for DDR52 (high speed 52MHz) for eMMC?
And for HS200?

Is the first 3.3V? May i use 3.3 both for DDR52 and HS200?

ラベル(1)
タグ(4)
2 返答(返信)

2,028件の閲覧回数
gusarambula
NXP TechSupport
NXP TechSupport

Hello Massimo Romano,

The supply voltage can be either 1.8V or 3.3V. However, 1.8V operation is limited by speed by Erratum 010450 (you can find it on the link below) so you would need to use 3.3V.

https://www.nxp.com/docs/en/errata/IMX6ULLCE.pdf

I hope this helps!

Regards,

2,028件の閲覧回数
massimo2
Contributor III

Thanks

0 件の賞賛
返信