I.MX6 ULL eMMC VDD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6 ULL eMMC VDD

2,153 Views
massimo2
Contributor III

Hello

What is the supply voltage used for DDR52 (high speed 52MHz) for eMMC?
And for HS200?

Is the first 3.3V? May i use 3.3 both for DDR52 and HS200?

Labels (1)
Tags (4)
2 Replies

2,010 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Massimo Romano,

The supply voltage can be either 1.8V or 3.3V. However, 1.8V operation is limited by speed by Erratum 010450 (you can find it on the link below) so you would need to use 3.3V.

https://www.nxp.com/docs/en/errata/IMX6ULLCE.pdf

I hope this helps!

Regards,

2,010 Views
massimo2
Contributor III

Thanks

0 Kudos
Reply