I.MX6 Pin Muxing Configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX6 Pin Muxing Configuration

3,024件の閲覧回数
vigneshvasudeva
Contributor II

Hi there,

We are using I.MX6 Quad Processor in one of our applications. Let me know if there are any Excel Sheets readily available to ease the Pin Muxing configuration of same.

This will help us in providing the hardware configuration document to the device driver development team. I had gone through the Pin Muxing details available in the Processor reference manual but I am not finding it easy to reuse in MS Excel to prepare Pin Mapping.

ラベル(1)
タグ(3)
2 返答(返信)

2,214件の閲覧回数
bipinbhatt
Contributor II

Hi Vignesh,

You can use IOMUX tool (iomux_tool_v3.4.0.3) for pin multiplexing and then you can export (File->Export) it to excel file.

The tool is available on freescale website.

Thanks & Regards,

Bipin

2,214件の閲覧回数
SergioSolis
NXP Employee
NXP Employee

Hello,

Sorry, but the information you are requesting is treated as confidential info at this time and requires a signed NDA (Non-Disclosure Agreement). Naturally, we cannot discuss this with you in public anyway, this requires to be handled as a Service Request (SR). Be aware that to give you remote support through a SR, we will still need the confirmation of a Freescale employee that the NDA is in place. If you want to go this route, the next steps will be: If you have already signed a NDA agreement for this product, please contact the person who assisted you or create a SR and name us a Freescale person that can confirm this. If you have not signed an agreement, please contact your local Freescale Distributor Salesperson or FAE for assistance. For a listing of our distributors, refer to: http://www.freescale.com/webapp/sps/site/overview.jsp?code=DISTRIBUTORS

Best regards,
Sergio

-------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-------------------------------------------------------------------------------

0 件の賞賛
返信