[I.MX536]Not enough data in ALSA buffer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[I.MX536]Not enough data in ALSA buffer

1,805件の閲覧回数
inuyasha
Contributor I

Dears,

Our platform is imx536, audio codec ak7757. when do playback, print out the following log:

ya_imxesai ya_imxesai.0: TX#1 Not enough data in ALSA buffer (256 frames)

I don't know this is a warning or err, but our media playback is normal. So this have any effects on us?

We also have ipod music fuction, our local media playback is normal, but our ipod music can't playback.

I do some works as follow:

1. I have check audio route is ok, local media playback and ipod music switch to  "ASP MEDIA Route" when do playback.

2. I capture PCM datas of local media and ipod music, found the PCM data of ipod music have nothing by Cool Edit.

What can i do, guys?:smileycry:

ラベル(2)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,673件の閲覧回数
joanxie
NXP TechSupport
NXP TechSupport

for IPOD, did you use usb audio? I found two patch for ipod playback, but I don't  know if they are useful for you, but you can refer to them.

<kernel/git/torvalds/linux.git - Linux kernel source tree  >.

<kernel/git/torvalds/linux.git - Linux kernel source tree >.

0 件の賞賛
返信

1,673件の閲覧回数
inuyasha
Contributor I

Hi, Guanqiong

Yes, we are debugging usb audio func, we had capture pcm data for ipod playback, found the pcm data have nothing!

0 件の賞賛
返信