I.MX23 LRADC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX23 LRADC

1,800件の閲覧回数
sujathap_m_
Contributor I

Hello,

I am using i.MX233 EVK from FSL ,and the Linux 2.6.31.

I am using LRADC channel 1 to read potentiometer voltage. I am able to read LRADC channel 1,but which is giving constant values(529/530/531). Is this channel internally configured to read some other voltages? If it is so how to deconfigure that ?

Regards,

Sujatha

0 件の賞賛
返信
1 返信

1,598件の閲覧回数
Paul_Kang
NXP Employee
NXP Employee

Sujatha,

LRADC1 channel is connected to external MIC for MIC bias in EVK board. Why do you want to read external voltage value at this channel?

Do you want to measure external voltage from LRADC1 channel without MIC function, right?

Best regards,

Paul

0 件の賞賛
返信