I.MX 6( MCIMX6S5EVM10ADR) BPM Microsystem programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX 6( MCIMX6S5EVM10ADR) BPM Microsystem programming

2,798件の閲覧回数
marco_villasana
Contributor I

Good afternoon, we are using the I.MX 6 in some of our products, we are currently using the NXP Mfg tool to program this device on board. We are willing to move this programing to a device level, prior to mounted on PCB, is it possible to program this micro using a programmer? (BPM machine in this case)

ラベル(1)
0 件の賞賛
返信
6 返答(返信)

2,743件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Marco

i.MX6 have not internal program flash, they use external media like

sd, or nor which may be programmed using programmer.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,743件の閲覧回数
marco_villasana
Contributor I

Thank you for your answer What about IMX8?

Regards!

0 件の賞賛
返信

2,743件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

it is the same

Best regards
igor

0 件の賞賛
返信

2,743件の閲覧回数
marco_villasana
Contributor I

Thank you for the quick answer, so, just to be clear, the IMX6 and IMX8 can not be programmed using any kind of programmer right?

0 件の賞賛
返信

2,743件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

right.

0 件の賞賛
返信

2,743件の閲覧回数
marco_villasana
Contributor I

Thanks for your attention

0 件の賞賛
返信