How we can invalidation the Power saving state in PCIe Gen1?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How we can invalidation the Power saving state in PCIe Gen1?

1,339 Views
toshihiro_kambe
Contributor II

Hi community

I am using a custom board that design based on NXP i.MX6Q sabreauto board,
and we need to run PCIe device on our custom board.

We must use Yocto Sumo(linux kernel 4.14.78) environment.
We would like to invalidation the Power saving state of PCIe(L0s,L1).

How we can invalidation the Power saving state(not transition from L0) in PCIe Gen1?

Best regards,
Toshihiro Kambe

Labels (2)
0 Kudos
Reply
1 Reply

1,293 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi Toshihiro ,

   L1 & L0s are not related to GEN1/GEN2. For PCIE, as long as RC and EP support it, it can be enabled.

Have a nice day!

B.R,

weidong

0 Kudos
Reply