How to write Boot_Mode[1:0] register to select internal boot

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to write Boot_Mode[1:0] register to select internal boot

2,345 次查看
adityanagal
Contributor III

Hi ,

I am working over IMX6 solo processor , as per reference manual  Boot_mode[1:0] should be written 0b10 to select the internal boot. So how to write to write the Boot_Mode[1:0] bits , so processors boot up with Internal boot . Thanks!

Regards,

Aditya Nagal

3 回复数

2,132 次查看
jan_spurek
NXP Employee
NXP Employee

Hello Aditya,

as an alternative, you can also set the Boot Mode register by adding pull up and pull down resistors or switches (as it is on our reference boards) to BOOT_MODE0 and BOOT_MODE1 pins.

bmode.png

Berst Regards,

Jan

2,132 次查看
adityanagal
Contributor III

Thanks a lot!!

0 项奖励
回复

2,132 次查看
diegoadrian
NXP Employee
NXP Employee

Hello Aditya,

Thank you for writing.

If you want to configure the Boot_Mode[1:0] register, the register needs to be written by J-tag.

I hope this can solve your question.

Best Regards,

Diego.

0 项奖励
回复