I need to drive a EPD with the iMX6SLEVK. I connect the pins to EPDC expansion port on iMX6SLEVK as follow .
EPD pins ------ iMX6SLEVK expansion port
VCOM ------ EPDC_VCOM0
BORDER ------ EPDC_BDR0
D0~D15 ------ EPDC_D0~EPDC_D15
CKH(clock source driver) ------ EPDC_SDCLK_P
LEH(latch enable source driver) ------ EPDC_SDLE
OEH(output enable source driver) ------ EPDC_SDOE
STH(start pulse source driver) ------ ?
MODE1(output mode selection gate driver) ------ ?
STV(start pulse gate driver) ------ EPDC_GDSP
CKV(clock gate driver) ------ EPDC_GDCLK
Now,my questions :
1 There are two pins I don't know how to connect.
2 Is right the other pins out?
3 How to use the last some pins on EPDC expansion port on iMX6SLEVK like EPDC_PWRCTRL EPDC_SDCE etc?
4 Where can I find the reference design of the IMXEBOOKDC3-E?
Thank you!