Dear Team,
I am using i.mx6sololite processor for our epos terminal. My question is can i use older version of uboot (NO device tree support i..e. 2009.08 uboot) wth newer version of kernel (i..e 3.10 kernel).what are the changes i need to todo .
and one more thing is i want to load kernel and dtb file combined .kindly let me know the memory locations changes for uImage loading (3.10 kernel ) with out dtb file loading separately.
Regards,
chandana.
Hi chandana
one can try to debug it using AN4553 Using Open Source Debugging Tools for Linux on i.MX Processors
http://www.nxp.com/assets/documents/data/en/application-notes/AN4553.pdf
Best regards
igor
hi Aravind,
I have gone through the document already.But i need to combine my DTB file along with kernel Image .that too i want to boot uboot 2009.08 with 3.10 kernel.
i have prepared uImage along with dtb but my kernel stucks at starting kernel....and not proceeding further.
so i doubt my uboot environment he am attaching my uboot related stuff.
bootdelay=1
baudrate=115200
loadaddr=0x80800000
rd_loadaddr=0x81000000
netdev=eth0
ethprime=FEC0
uboot=u-boot.bin
kernel=uImage
nfsroot=/opt/eldk/arm
bootargs_base=setenv bootargs console=ttymxc0,115200
bootargs_nfs=setenv bootargs ${bootargs} root=/dev/nfs ip=dhcp nfsroot=${serverip}:${nfsroot},v3,tcp
bootcmd_net=run bootargs_base bootargs_nfs; tftpboot ${loadaddr} ${kernel}; bootm;
bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk0p1 rootwait quiet 
bootcmd_mmc=run bootargs_base bootargs_mmc; mmc dev 1; mmc read ${loadaddr} 0x800 0x4000; mmc read 0x98000000 0x4A00 0x12C; bootm
bootcmd=run bootcmd_mmc
bootdelay=1
ethact=FEC0
ver=GL11-UB-2009.08-1173-1.0.bin (Jun 14 2016 - 15:34:52)
first_boot=1
boot_fdt=no
filesize=5164C9
fileaddr=80800000
ipaddr=192.168.2.39
and am stucking at
 bootm
## Booting kernel from Legacy Image at 80800000 ...
   Image Name:   Linux Kernel
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    5334153 Bytes =  5.1 MB
   Load Address: 80800000
   Entry Point:  80800000
   Verifying Checksum ... OK
   XIP Kernel Image ... OK
OK
Starting kernel ...
After this message is not booting.
kindly guide me.
Regards,
chandana
Hi Chandana,
Take below environment as reference:
| => | |
| baudrate=115200 | |
| bootaddr_dl=0x10008000 | |
| bootaddr_sys=0x10008000 | |
| bootargs=console=ttymxc0,115200 root=/dev/mmcblk2p2 rootfstype=ext4 rootwait rw fixrtc | |
| bootargs_all=console=ttymxc0,115200 | |
| bootargs_app=quiet | |
| bootargs_sys=rw root=/dev/mmcblk1p2 rootfstype=ext4 rootwait | |
| bootcmd=mmc start;fatload mmc 1:1 0x11200000 imx6q-sabresd.dtb;fatload mmc 1:1 0x12800000 uImage; bootm 0x12800000 - 0x11200000 | |
| bootdelay=1 | |
| console=ttymxc0,115200 | |
| dbootcmd_app=run loadfdt; bootm $bootaddr - $fdt_addr | |
| dbootcmd_dl=run loadfdt; run loadrd; bootm $bootaddr $rd_addr $fdt_addr | |
| dbootcmd_srv=run loadfdt; bootm $bootaddr - $fdt_addr | |
| ethact=FEC | |
| ethaddr=00:04:9f:02:6a:b2 | |
| ethprime=FEC | |
| fdt_addr=0x11000000 | |
| fdt_high=0xffffffff | |
| fdtfile=dtb | |
| fdtfile_dl=dtb-dl | |
| fdtfile_sys=dtb | |
| filesize=5b4750 | |
| initrd_file=uInitrd | |
| initrd_high=0xffffffff | |
| kernel_file=uImage | |
| kernel_file_dl=uImage-dl | |
| loadaddr=0x10008000 | |
| loadfdt=fatload mmc ${mmcdev}:${mmcpart} ${fdt_addr} ${fdtfile} | |
| loadrd=fatload mmc ${mmcdev}:${mmcpart} ${rd_addr} ${rdfile} | |
| mmcdev=0 | |
| mmcpart=1 | |
| panel=HDMI | |
| rd_addr=0x11200000 | |
| rdfile=uInitrd | |
| verify=n | 
Regards,
Aravinth