How to use kdump in signed kernel

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use kdump in signed kernel

1,895件の閲覧回数
Raana
Contributor III

Dear Team,

Currently, I'm using i.Mx8x based custom board. BSP version is, imx-yocto-L4.14.98_2.0.0_ga.

My query is, I want to capture the crash log when the kernel is getting crash/panic. 

We are using 'kdump' utility to achieve this.

Here, I'm using signed (Image + signature) container (combination of Image and dtb).
This signed container will get authenticate and extract in Uboot (by using "auth_cntr") for normal boot.

There are two kernels,
- Standard (production) kernel - kernel we normally boot
- Crash (capture) kernel - kernel specially used for collecting crash dumps

I want to use the signed container for capture kernel also. As per kdump, the capture kernel will be booted from standard kernel

when the crash/panic occurred.


Is there any possibilities to extract the signed capture kernel in standard kernel?

Thank You.
Best Regards,
J.P.Raja

ラベル(2)
0 件の賞賛
返信
1 返信

1,827件の閲覧回数
b36401
NXP Employee
NXP Employee

Here is an article regarding to kdump usage:
https://community.nxp.com/docs/DOC-347175

0 件の賞賛
返信