How to use CAN bus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to use CAN bus

1,854 次查看
kishorekrish
Contributor I

Hi,

I have IMX6 board,i want to know what is the exact need of CAN bus on IMX6 and how i use it i.e how to connect with other interfaces like cars etc, please explain .

Thank you.

0 项奖励
回复
1 回复

1,650 次查看
art
NXP Employee
NXP Employee

To connect your i.MX6-based board to a car over the CAN bus using OBD-II car protocol, you first have to connect your i.MX6 board's CAN bus to the CAN bus of the car's OBD-II connector:

https://en.wikipedia.org/wiki/On-board_diagnostics

Then, you have to study the OBD-II protocol:

https://en.wikipedia.org/wiki/OBD-II_PIDs

And then you have to start entering PIDs from the processor and receiving parameters from the car's ECU and other systems.

You can google much more in the internet on that matter.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复