How to use CAN bus

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use CAN bus

1,851件の閲覧回数
kishorekrish
Contributor I

Hi,

I have IMX6 board,i want to know what is the exact need of CAN bus on IMX6 and how i use it i.e how to connect with other interfaces like cars etc, please explain .

Thank you.

0 件の賞賛
返信
1 返信

1,647件の閲覧回数
art
NXP Employee
NXP Employee

To connect your i.MX6-based board to a car over the CAN bus using OBD-II car protocol, you first have to connect your i.MX6 board's CAN bus to the CAN bus of the car's OBD-II connector:

https://en.wikipedia.org/wiki/On-board_diagnostics

Then, you have to study the OBD-II protocol:

https://en.wikipedia.org/wiki/OBD-II_PIDs

And then you have to start entering PIDs from the processor and receiving parameters from the car's ECU and other systems.

You can google much more in the internet on that matter.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信