How to update 1G DDR3 to 2G DDR3 on i.MX6QSabresd board 3.14.52

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to update 1G DDR3 to 2G DDR3 on i.MX6QSabresd board 3.14.52

跳至解决方案
4,562 次查看
浩卢
Contributor III

hi:

How to update 1G DDR3 to 2G DDR3 on i.MX6QSabresd board.What should I do with uboot ?

Now I am using  the version yocto 3.14.52.u-boot version is 2015.04.

I have try to do some change like this How to update 1G DDR3 to 2G DDR3 on i.MX6QSabresd board

ddr change.png

But it doesn't work. It is still 1G size DDR. Here is the log

U-Boot 2015.04-imx_v2015.04_3.14.52_1.1.0_ga+g6cf684a (Apr 20 2016 - 16:01:47)

CPU:   Freescale i.MX6Q rev1.2 at 792 MHz

CPU:   Temperature 31 C

Reset cause: POR

Board: MX6-SabreSD

I2C:   ready

DRAM:  1 GiB

PMIC:  PFUZE100 ID=0x10

MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2

*** Warning - bad CRC, using default environment

No panel detected: default to Hannstar-XGA

Display: Hannstar-XGA (1024x768)

In:    serial

Out:   serial

Err:   serial

switch to partitions #0, OK

mmc2(part 0) is current device

Net:   FEC [PRIME]

Error: FEC address not set.

Normal Boot

Hit any key to stop autoboot:  0

标签 (3)
0 项奖励
回复
1 解答
3,242 次查看
igorpadykov
NXP Employee
NXP Employee

please run ddr test

i.MX6/7 DDR Stress Test Tool V2.52

and update uboot/../mx6sabresd/mx6q_4x_mt41j128.cfg

with new parameters obtained from ddr test

Best regards

igor

在原帖中查看解决方案

5 回复数
3,242 次查看
sywksmstkadlfgk
Contributor III

and update uboot/../mx6sabresd/mx6q_4x_mt41j128.cfg

with new parameters obtained from ddr test

3,243 次查看
igorpadykov
NXP Employee
NXP Employee

please run ddr test

i.MX6/7 DDR Stress Test Tool V2.52

and update uboot/../mx6sabresd/mx6q_4x_mt41j128.cfg

with new parameters obtained from ddr test

Best regards

igor

3,242 次查看
浩卢
Contributor III

Thank you igorpadykov .

0 项奖励
回复
3,242 次查看
Yuri
NXP Employee
NXP Employee

Hello,

Please use Chapter 1 (Porting U-Boot from an i.MX 6/7 Reference Board to

an i.MX 6/7 Custom Board) of "i.MX_BSP_Porting_Guide.pdf" in Linux docs.

< http://www.nxp.com/webapp/Download?colCode=L3.14.52_1.1.0_LINUX_DOCS >

Also, the following may be helpful.

"Freescale i.MX6 DRAM Port Application Guide-DDR3"

< https://community.freescale.com/docs/DOC-101708 >

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
3,246 次查看
浩卢
Contributor III

Thank you Yuri Muhin.

0 项奖励
回复